Technical FAQs

Ask a Question

Is the transducer sensor included with the E-FLEX C09 option?

Issue:
What is included with the E-FLEX C09 option?

Product Line:
8839 E-FLEX

Environment:
All

Cause:
Clarification of what is included with C09 option.

Resolution:
Modification C09 is an option for a 3–15PSI Transducer with Digital Display.  This option provides the E-Flex controller with a transducer that accepts a user-supplied
3–15 PSI follower signal.  The transducer displays the input pressure value. The module is calibrated to operate as a 4–20mA DC follower for the power converter.

A transducer sensor that creates the 3-15PSI signal is not included.
Was this helpful?
What can we do to improve the information ?