Technical FAQs

Ask a Question

E-Flex Product selector: Attempt to add a line contactor is not allowed.

Issue: 
Selecting an E-Flex and the line contactor option is not allowed.

Product Line:
E-Flex drives

Environment: 
All serial numbers for E-Flex drives

Cause: 
Conflicting options

Resolution: 
The Line Contactor option is not avaliable with Power Circuit W (Without Bypass).  Consider M-Flex which offers specials.

Was this helpful?
What can we do to improve the information ?