Technical FAQs

Ask a Question

Does Schneider Electric offer a stand alone NEMA 4X drive or soft starter?

Issue:
Does Schneider Electric offer a stand alone NEMA 4X drive or soft starter?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Special enclosure option

Resolution:
Schneider Electric doesn't offer a stand alone NEMA 4X enclosed drive or soft starter in the US. 
Type 4 or 4X is not a standard offering. The drives are available in a Type 1, Type 12 and a Type 3R enclosures. 

Some special products can be built.
Contact your local SquareD field office or Drive PAE for more information. They can contact Drives Quotation Group to develop a quote.
Was this helpful?
What can we do to improve the information ?