Technical FAQs

Ask a Question

Are the Kirk keylocks for Masterpact NW and NT breakers the same?

Issue:
Do the Masterpact NW and NT circuit breakers use the same Kirk keylocks?

Product Line:
Masterpact NW, Masterpact NT

Environment:
Electrical Distribution Systems

Cause:
Occasionally customers want to move a key interlock from one circuit breaker to another.

Resolution:
Yes, the locks are the same, but they have different provisions for installation on the breaker.
Kirk Single Lock CN22-1.2 (Square D Part # 35635)
Was this helpful?
What can we do to improve the information ?