Technical FAQs

Ask a Question

What size circuit breaker is used in an Enclosed 48 soft starter?

Issue:
What size circuit breaker is used in an Enclosed 48 soft starter?

Product Line:
Altistart ATS48 enclosed

Environment:
All 48 Enclosed

Cause:
circuit breakers used on the enclosed 48U soft starters.

Resolution:
Determine the Voltage and Horsepower of the soft starter and refer to table 10 in section 6 replacement parts in Document 30072-450-62B.

Was this helpful?
What can we do to improve the information ?