Technical FAQs

Ask a Question

Invalid reply error message on RSLogix when configuring an ATV61 or ATV71 with ethernet IP card.

Issue:
Invalid reply error on  RSLogix configuring an ATV61 or ATV71 with ethernet IP card.

Product Line:
Altivar ATV61 and ATV71

Environment:
VW3A3316 ethernet IP card on the ATV61 or ATV71 drives

Cause:
RSLogix is configured for double integer

Resolution:
Set up RSLogix configuration for single integer.
Using assemblies 100 and 101.
Was this helpful?
What can we do to improve the information ?