Technical FAQs

Ask a Question

What are the cooling fan kit part numbers for an E-flex system with an ATV61HD22N4 drive?

Issue:
What is the cooling fan kits part numbers for an E-flex  with an ATV61HD22N4 drive?

Product Line:
ATV61  Altiar 61
 
Environment:
ATV61HD22N4
 
Cause:
Part number needed to order part
 
Resolution:
The heat sink fan part number is VZ3V1211
The stirring fan assembly  part number is a 31158-065-50
3R ventilation fan part number is 26016-00006
Was this helpful?
What can we do to improve the information ?