Technical FAQs

Ask a Question

Can the configuration file of an ATV66 drive be copied to an ATV61/71 drive?

Issue:
The customer needs to copy the configuration from an ATV66 to an ATV61/71

Product Line:
ATV66, ATV61 ATV71

Environment:
All models and serial numbers

Cause:
Customer is replacing the ATV66 with an ATV61 and needs to program the new drive.

Resolution:
It is not possible to copy the configuration file from an ATV66 into the ATV61/71.  It must be done manually.
Was this helpful?
What can we do to improve the information ?