Technical FAQs

Ask a Question

What parts are needed to upgrade a PowerPact P or R frame breaker from a standard trip unit to a Micrologic 3.0A 5.0P 6.0P 5.0H or 6.0H?

Issue:
What parts are needed to upgrade a PowerPact P or R frame breaker from a standard Micrologic trip unit to a Micrologic 3.0A 5.0P 6.0P 5.0H or 6.0H?

Product Line:
PowerPact P and R frame

Environment:
Electrical Distribution Systems

Cause:
A customer may want to increase the functionality of their trip unit

Resolution:
Choose the appropriate trip unit:
3.0A S141A
5.0A S143A
6.0A S144A
5.0P S163A
6.0P S164A
5.0H S173A
6.0H S174A

For R frame and for P frame (excluding motorized, rotary handle, and drawout), they also need the following parts:
Connector S33100
External Voltage Sensing kit S64203 (P and H trip units only, if Voltage sensing is required)
BCM S64205 (if modbus is required)

For P frame drawout, they need the following parts:
Connector S33101
External Voltage Sensing kit S64209 (P and H trip units only, if Voltage sensing is required)
BCM S64206 (if modbus is required)

For P frame motorized, they need the following parts:
Connector S33100
External Voltage Sensing kit S64210 (P and H trip units only, if Voltage sensing is required)
BCM S64207 (if modbus is required)

For P frame with rotary handle, they need the following parts:
Connector S33100
External Voltage Sensing kit S64210 (P and H trip units only, if Voltage sensing is required)
BCM S64205 (if modbus is required)

NOTE:  if upgrading to a 6.0x trip unit (one with ground fault protection) or to a 5.0P/H trip unit used for ground fault alarm) on a 4-wire system (with a neutral) it is also necessary to install a neutral CT.  
Refer to the current edition of Digest section 7 for the appropriate NCT for Powerpact, and to the Masterpact Pricing Guide 0613PL0001 for the appropriate NCT for Masterpact breakers.
Was this helpful?
What can we do to improve the information ?