Technical FAQs

Ask a Question

Does mounting hardware come with Power Distribution Connector (PDC) lug kits?

Inquiry:
What comes in the kit with Power Distribution Connectors?

Product Line:
Legacy and Powerpact circuit breakers

Environment:
UL 508 control panels and OEM applications

Resolution:
The instructions bulletin 48040-929-04 (attached) and all of the hardware required for proper installation is included in the kit.
Kit Contents
• Power Distribution Connectors
• Lug Mounting Screw(s)
• Special Purpose Label
• Lug Data Label
• Lug Pack Cover (D-, L-Frame)
• Lug Pack Base (D-, L-Frame)
Was this helpful?
What can we do to improve the information ?