Technical FAQs

Ask a Question

How do you obtain, install, use, and troubleshoot LTU software for the UTA tester for Powerpact H, J, and L frame circuit breakers?

Product Line:
Powerpact H, J, L circuit breakers and UTA tester

Environment:
Windows XP and Windows 7 ONLY!  
Incompatible with Windows 8 and 10

Resolution: 
  1. Download the software from this link:  http://www.schneider-electric.com/en/download/document/Micrologic_LTU_Rev_9.2.2_Setup/
    • Reboot computer
    • If UTA tester was already connected and/or powered up, disconnect from computer and from wall outlet for 20 seconds.  Then reconnect and proceed.
  2. Connect the UTA tester to the computer and the circuit breaker trip unit, per Help File instructions in the software. 
  3. Click on Setup and then on PC communication parameters,  Ensure Channel is set to USB Maint. Module and the Serial port name to Com4:  Maintenance Module.  It may use a different number com port such as Com1, Com2, etc.  Click OK.
  4. (3) Next click on Remote Functions and Get Micrologic Settings.  OK the identification form dialog box.  Filling in identification is optional.  The Serial Number should fill in automatically.  If it doesn't, fill it in manually.
  5. (4) Click on Manual TEST or Automatic TEST for secondary injection testing.
  6. (5) To save a test report, click on File and Display Report.
  7. If problems are encountered with these steps, consult Article FA235058
  8. Refer to the HELP FILES in the Help menu for more details on the test procedure.
Was this helpful?
What can we do to improve the information ?