Technical FAQs

Ask a Question

Is it possible to field install the DC choke on the D version of the ATV61HD90N4D drives?

Issue: 
Is it possible to field install the DC choke on the D version of the ATV61HD90N4D drives?

Product Line:
Altivar 61, ATV61

Environment:
ATV61HD90N4D

Cause:
The AV61HD90N4D was ordered which ships without the DC choke.

Resolution:
The DC choke for this part is not available for sale. Recommended solution is to add a 5% input line reactor, separately mounted. 
Was this helpful?
What can we do to improve the information ?