Technical FAQs

Ask a Question

What connection or termination options are available for Powerpact H, J, and L frame circuit breakers?

Product Line:
Powerpact H, J, L circuit breakers

See the the attachment for available termination options which include:  rear connections, mechanical lugs (with or without control wire taps/voltage takeoffs), compression lugs, busbar connection, and power distribution lugs.
Was this helpful?
What can we do to improve the information ?