Technical FAQs

Ask a Question

What does the LH2 suffix mean for catalog number LGP36250U31XLH2?

Issue:
What does the LH2 suffix mean on a PowerPact L frame breaker?

Product Line:
PowerPact L Frame Breakers

Environment:
This covers all unit mount PowerPact L frame breakers.

Cause:
Need to determine how to specify certain lugs for PowerPact L frame breakers.
 
Resolution:
The LH2 suffix is for the lug with the floating wire binding screw which will accept (2) 3/0 AWG to 500kcmil AL or CU cables.

 
Was this helpful?
What can we do to improve the information ?