Technical FAQs

Ask a Question

How can an address be set in the ATV58 drive when working with ATV58 InterBus communication?

Issue:
How can an address be set in the ATV58 drive when working with ATV58 InterBus communication?

Product Line:
Altivar ATV58

Environment:
All

Cause:
All

Resolution:
The Interbus-S communication protocol does not have individual drive addresses. However, the location of the drive in the daisy chain is important. The Master controller i.e. PLC will take care of the addressing.
 

Was this helpful?
What can we do to improve the information ?