Technical FAQs

Ask a Question

Why my PDP does not align with my Conduit Box on the circular openings?

The Conduit box has several openings. However, the conduit box only communicates with the PDP through the large rectangular opening on the top of it. The circular conduit box openings are meant for the connections when you have multiple XW inverters.

Here is an image that depicts the mismatch of the circular openings for the conduit and the PDP


Here is a picture of the correct way to communicate between the XW PDP and the conduit box. 

Was this helpful?
What can we do to improve the information ?