Technical FAQs

Ask a Question

How do I enable automatic restart on my ATV61 E-flex system?

Issue:
How do I enable automatic restart on my ATV61 E-flex system?

Product Line:
Altivar 61 Eflex

Environment:
All models, All serial numbers

Cause:
Directions needed to enable automatic restart

Resolution:
In order to enable automatic restart, the drive must be in 2 wire control mode and parameter 2 wire control type must be set to level. Once this is done, navigate to menu 1.8, Fault management and set parameter automatic restart to Yes. 
Was this helpful?
What can we do to improve the information ?