Technical FAQs

Ask a Question

What is the speed accuracy of the ATV12 drive in sensorless flux vector control mode?

Issue:
What is the speed accuracy of the ATV12 drive in sensorless flux vector control mode?

Product Line:
Altivar ATV12

Environment:
All

Cause:
speed accuracy of the drive.

Resolution:
The accurate speed is 2% accuracy between no load condition and nominal load conditions.

 
Was this helpful?
What can we do to improve the information ?