Technical FAQs

Ask a Question

What is the part number for a heat sink fan for ATV61HC22N4 and ATV71HC20N4?

Issue:
What is the part number for the heat sink fan for ATV61HC22N4 and ATV71HC20N4?

Product Line:
ATV61HC22N4, ATV61HC20N4, ATV71HC22N4 and ATV71HC20N4

Environment:
All serial numbers for ATV61HC22N4, ATV61HC20N4, ATV71HC22N4 and ATV71HC20N4

Cause:
Part number needed to order heat sink fans

Resolution:
VZ3V1212 is the part number for the heat sink fan at the bottom of the drive. 
Please note if you replace the cooling fan VZ3V1212 you will also need to replace the fan control board part number VX5A1400 too.
This applies to ATV61 and ATV71 frame sizes 10 thru 15.

Was this helpful?
What can we do to improve the information ?