Technical FAQs

Ask a Question

Requesting a fingersafe cover for a 60274 multi 9 breaker

Issue:
Request to field install a fingersafe cover on a Multi 9 breaker in the field.

Product Line:
Multi 9 C60 Breakers

Environment:
Applies to Multi 9 breakers.

Cause:
An installed Multi 9 breaker needs fingersafe guards.

Resolution:
The fingersafe cover can only be factory installed on the Multi 9 C60 breakers by adding an "F" to the end of the catalog number..
Was this helpful?
What can we do to improve the information ?