Technical FAQs

Ask a Question

How do I connect XW AGS to Kohler 14/20RES generators?

Kohler generators have a remote terminal located on the back side of the unit (position 3 & 4). This is a simple on/off setup. It does not require a voltage to have the unit operate.







Type 14 can be used to provide the continuity to start the generator across pins 14 & 16. No run signal is required.





 

 

Was this helpful?
What can we do to improve the information ?