Technical FAQs

Ask a Question

Where can I find the XW inverter series CSA Certificate as well as the Commissioning instructions?

CSA Certificate and Commissioning Instructions

In this article you will be able to find the CSA certificate for all XW units including XW048, XW4548, as well as XW4024. Also You will find the specifications for each unit as well as the Commissioning Instructions and commissioning test for the unit, which should serve as a period test since it tests all the safety features in regards to grid interconnect. 

Specifications 
Was this helpful?
What can we do to improve the information ?