Technical FAQs

Ask a Question

How long are the battery cables that ship with the XW Power Distribution Panel 865-1015-01?

Positive 4/0 battery cable with PDP is 0.86m (34.0 in.)
Negative 4/0 battery cable with PDP is 0.76m long (30.5 in.) 

THESE CONNECT FROM THE XW+NA INVERTER TO THE PDP POS AND NEG BUSES. 
CABLES FROM PDP TO BATTERY MUST BE SOURCED BY THE CUSTOMER AS DIFFERENT LENGTHS ARE REQUIRED.
Was this helpful?
What can we do to improve the information ?