Technical FAQs

Ask a Question

What are the default charger settings for a Conext SW?

What are the default charger settings for a Conext SW?



SW 2524 120/240 

Batt Type - Flooded
Batt Capacity - 250Ah
Max Chg Rate - 100%
Charge Cycle - 3stage
ReCharge Volts - 25.0V
AC In Breaker - 30A
Low Batt Cut Out - 21.0V


SW 4024 120/240 

Batt Type - Flooded
Batt Capacity - 440Ah
Max Chg Rate - 100%
Charge Cycle - 3stage
ReCharge Volts - 25.0V
AC In Breaker - 30A
Low Batt Cut Out - 21.0V
 
Was this helpful?
What can we do to improve the information ?