Technical FAQs

Ask a Question

What do the PV terminals of a GT unit look like (ABB disconnect)?

GT Unit Terminals 



This is the DC side or the PV input. Notice that in this GT accepts two strings of PV panels 







This is the AC Side of the unit. Notice that it is located on the opposite side of the GT





 
Was this helpful?
What can we do to improve the information ?