Technical FAQs

Ask a Question

Conext XW+ Series Inverters - W95 Equalize Abort

Conext XW+ Series Inverters - W95 Equalize Abort


Unit is faulting during equalization and aborts the equalize process due to dropped transfer, unit displays a W95. 

This unit is faulting because the AC source is lost, wait until AC input (utility grid) returns to in-tolerance condition.

This can also occur if the conductors are undersized for distance, creating voltage drop. It may be necessary to lower the AC input voltage lower limit (Advanced Settings>AC Settings).

This could also happen if you are using a generator that is not correctly size for the system causing the generator to over load.
Was this helpful?
What can we do to improve the information ?