Technical FAQs

Ask a Question

What are the Conext XW and Conext SW inverter specifications?

Conext XW and SW Inverter Specifications 


Here are the specifications for the Conext XW units, this includes the XW6048, the XW4548, and the XW4024



Here are the specs for the Conext SW series, including both SW4024 and SW2524



Was this helpful?
What can we do to improve the information ?