Technical FAQs

Ask a Question

What happens when you connect a MPPT 80-600 charge controller on a multiple unit installation on the xanbus network with the same device?

Multiple charge controllers connected to the same network will generate F69 if they have the same device number. The error will clear when the operator changes to a different device number for each controller. The device number can be changed in the Multi Unit Config screen of the SCP for the device that is to be configured.
Was this helpful?
What can we do to improve the information ?