Technical FAQs

Ask a Question

Can AL400LA lugs be installed on a LAF36400 breaker?

For LAF Molded Case Circuit Breakers, can lugs be added to this breaker for replacement?

Product Line:
LAF, LHF Molded Case Circuit Breakers

Applies to LAF, LAP, LHF, LHP Breakers that come with no lugs

An installed breaker with no lugs and the customer needs to purchase parts to add lugs to the breaker.

Yes, the AL400LA lugs will work on the LAF style breaker.
Lug kit - AL400LA (1) #1AWG-600kcmil or (2) #1 AWG-250kcmil (per lug);

Was this helpful?
What can we do to improve the information ?