Technical FAQs

Ask a Question

Why is my C60 charge controller labeled as a C40 inside the unit?

PCB p/n 2230E is used on BOTH the C40 and C60. The silkscreen might only say C40. The fact that the 48V jumper pins missing indicates this is in fact a C60.

This change only went into effect Mar 2013. 

Here are some images that show what the C60 looks like inside and the confusion between the C40 and the C60. 


      
Was this helpful?
What can we do to improve the information ?