Technical FAQs

Ask a Question

Where can I find information on the wire sizes for ATV71 for PO to PA terminals?

Issue:
Where can you find information on the wire sizes for ATV71 for PO to PA terminals?

Product Line:
ATV61 and ATV71

Environment:
All serial numbers for ATV61 and ATV71

Cause:
For how to size wires for the drive

Resolution:
Information for maximum wire sizes can be found in the ATV71 installation manual ATV71_Installation_manual_en_v1.

Was this helpful?
What can we do to improve the information ?