Technical FAQs

Ask a Question

How can you order an RL line reactor in a NEMA 1 enclosure?

What is the part number for a Nema 1 conduit kit for any line reactor?

Product Line:

All serial numbers for RL-XXXX

Part number needed to order

AC reactors are available as either open type or in a Nema Type 1 general purpose enclosure.  To order a reactor mounted in a cabinet simply change the second last digit of the part number from "0" to "1". 
Example RL-00802 becomes RL-00812

Was this helpful?
What can we do to improve the information ?