Technical FAQs

Ask a Question

Can you run the ATV11 drive in local mode off the face of the drive?

Issue:
Can you run the ATV11 drive in local mode off the face of the drive?

Product Line:
Altivar ATV11

Environment:
All

Cause:
Needs to run the drive from local mode

Resolution:
No the standard U suffix ATV11 does not have local controls.  Please note there is an Asian version with a A suffix that does have local speed control and run stop but its not sold in the USA.
 

Was this helpful?
What can we do to improve the information ?