Technical FAQs

Ask a Question

What are the recommended lug wire-binding screw torque values for Powerpact H, J, L, M, P, R, QO, and FDL/EDB circuit breakers?

Product Line:
Powerpact, QO, EDB, FDL circuit breakers

Resolution:
Please see the attachment.
Note that while the values contained in the attachment were true at the time of publication, these values are subject to change and in case of a discrepancy, use the torque value printed on the breaker label. 
Was this helpful?
What can we do to improve the information ?