Technical FAQs

Ask a Question

How many circuits are needed to feed an EV230PDR or EV230PDRR?

Issue:
How many circuits are needed to feed an EV230PDR or EV230PDRR?

Product Line:
PTEVC - ELECTRICAL VEHICLE

Environment:
Electrical vehicle charging stations

Cause:
Information needed for installation

Resolution:
The EV230PDR and EV230PDRR are dual chargers in one unit. There will be two separate circuit required to feed these charging units. Each circuit should be fed by a 40A, 2 Pole, non-GFI type circuit breaker. The wiring should be #8 AWG.  A neutral connection is not required for EVlink Charging Stations.

You may also want to view a related FAQ: Feeder Circuit Requirements for EV Charging Stations

The installation manual: EV230PDR and EV230PDRR Installation Manual

More information on Schneider Electric EV Charging Stations
Was this helpful?
What can we do to improve the information ?