Technical FAQs

Ask a Question

Why is the low speed management bSP parameter not accessible in Menu 4?

Issue:
The low speed management (bSP) parameter is not accessible.

Product Line:
ATV58 and Flex58

Environment:
All models with firmware V2.1 IE06

Cause:
None

Resolution:
The bSP parameter was added in firmware level V3.1 IE14.

Was this helpful?
What can we do to improve the information ?