Technical FAQs

Ask a Question

Will Fault F55 clear it self or does it have to be cleared manually in the MPPT80?

The fault F55 will clear itself when the heat sink temperature falls below 80 °C (176 °F) for 30 seconds.
Was this helpful?
What can we do to improve the information ?