Technical FAQs

Ask a Question

How do I connect the C-series charge controller to a Wind Turbine?

 C-Series and Wind Turbines


The C-series is not meant to be used as a charge controller for wind turbines, the only approved usage of it with a wind turbine is as a Diversion Load controller. This function on the C-series is meant so that the wind turbines won't overcharge the batteries as there is no way of stopping the wind from blowing. It basically connect a load the same size of the wind turbine to the batteries when they are fully charge. Here is an example of the Diversion Load Control mode and wiring for it.


 
Was this helpful?
What can we do to improve the information ?