Technical FAQs

Ask a Question

Why can't my XW power a full load on one line?

The XW+NA models are configured for split-phase 120/240V from the factory, and can only support 75% of load rating on one line. It is possible to obtain full output on one line by "converting" to 120V.
Was this helpful?
What can we do to improve the information ?