Technical FAQs

Ask a Question

Can a AL175JD lug kit go on a J frame breaker greater than 175 amps ?

Product Line:
PowerPact J frame Molded Case Circuit Breakers

Environment:
Used with PowerPact J frame breakers rated greater than175A.

Resolution:
The AL175JD lug kit will work on the 200-250A J frame breakers. When ordering the PowerPact J frame breaker greater than 175A add suffix LY the the end of the catalog number to have the AL175JD lug factory installed.
Was this helpful?
What can we do to improve the information ?