Technical FAQs

Ask a Question

Does a HCM23642N panel have a ULSE label as standard and if so, where is it located ?

Issue:
UL Labeling

Product Line:
Panelboard

Environment:
I-Line

Cause:
Standard feature location

Resolution:
Yes. This should have a ULSE on the galvanized steel base of the interior .

Was this helpful?
What can we do to improve the information ?