Technical FAQs

Ask a Question

How can you choose an Altivar drive based on motor KW data not HP?

Issue:
How can you choose an Altivar drive based on motor KW data not HP?

Product Line:
All Altivar products.

Environment:
All

Cause:
Translation of differing standards.

Resolution:
1Kilowatt = 1.34102209 Horsepower.  As an example, the ATV71H075N4 is rated for .75KW and 1HP.   .75 * 1.34102209 = 1.0057 HP.
Was this helpful?
What can we do to improve the information ?