Technical FAQs

Ask a Question

When AC coupling the XW, which charge cycle should be selected?

The charge cycle (3Stage or 2Stage/No Float) should be set for whatever the battery manufacturer recommends (some manufacturers do not recommend floating their batteries).
Unlike Grid Support operation, which requires charge cycle to be set for 2Stage/No Float, the current produced by the grid tied inverter will pass thru the XW as long as AC transfer has occurred.
Was this helpful?
What can we do to improve the information ?