Technical FAQs

Ask a Question

Why does the XW+ inverter display a F66 F69 fault during a firmware upgrade?

If the units remain connected together (in a master/slave arrangement) during the firmware update process, the units could display a fault due to the multi-unit configuration, causing an interruption of the update process.

Please note the following fault descriptions:

F66 -  Multi-Unit Configuration settings are incorrect.
F69 -  External Sync Failed (Multi-Unit Configuration fault)

To resolve this issue, clear the fault and disconnect everything (XANBUS, AC sync Cable) from the unit that requires the firmware upgrade. This will help rule out any communication issue due to noise and bad cables. Then connect the configuration tool directly to the single unit and proceed with the update accordingly. 

 
Was this helpful?
What can we do to improve the information ?