Technical FAQs

Ask a Question

How do you size a circuit breaker for a motor load.

Product Line:
MCCBS OPTIMUM OFFER

Environment:
Applies to  Powerpact motor circuit protectors.

Resolution:
Breaker amperage is determined by the HP, voltage, phasing,and type of motor used. (There is usually a motor code stamped on the motor itself).

See attached files.
Was this helpful?
What can we do to improve the information ?