Technical FAQs

Ask a Question

What can cause an E-flex drive to trip on No Sensor T fault?

Issue:
Walmart E-flex drive is tripping on No Sensor T fault.

Product Line:
E-Flex Walmart Drive

Environment:
Walmart Custom built drives only

Cause:
Temperature sensor signal is out of range.

Resolution:
Power cycled the drive to see if the fault will reset. You will get No Sensor T fault if there is no temperature transmitter signal detected continuously for 15 minutes.

Also go into Menu 1.14 check the temperature ambient temp value. If there is no signal there or if the signal is out of range you may have a bad temp sensor.

Was this helpful?
What can we do to improve the information ?