Technical FAQs

Ask a Question

Will the E-Flex R1 relay function "Drive Start" apply when controlling with communications mode?

Issue:
Will the EFlex R1 relay function "Drive Start" apply when controlling with communications mode?

Product Line:
ATV61

Environment:
All

Cause
This function is needed with Apogee P1 control

Resolution:
Yes, R1 assignment "Drive Start " function works with communications controls.
Was this helpful?
What can we do to improve the information ?