Technical FAQs

Ask a Question

Is the ATV66 drive series still available? If not, what is the replacement?

Issue
The ATV66 series drives still available?
 
Product Line:
Altivar 66,  ATV66
 
Environment:
All
 
Cause:
The ATV66 drives were obsoleted in 2004.
 
Resolution:
 You can replace the ATV66 with the ATV71 for constant torque applications or ATV61/ATV630 for variable torque applications. Select drives base on application requirements for voltage, horsepower and current.
 

 

Was this helpful?
What can we do to improve the information ?