Technical FAQs

Ask a Question

Where can I find the serial number for my ATV61 or ATV71 drive?

Issue:
Where can I find the serial number on the product for ATV61 and ATV71 drives?

Product Line:
Altivar 61, Altivar 71, ATV61, ATV71

Environment:
All

Cause:
Serial number Identification, date code

Resolution:
Using the HMI display (VW3A1101), you can find the serial number for the drive in the Identification Menu, 1.11.  The path is Drive Menu > 1.11 Identification.  The 6th line from the top in this menu shows the drive serial number.  (The line after MC Software).

You can also find the serial number on the nameplate.  The nameplate is a sticker on the right side of the drive itself.  the serial number is located under the bar code and will begin with EL, 88, 8B or 6W.

Was this helpful?
What can we do to improve the information ?