Technical FAQs

Ask a Question

Will my C40 and MPPT60 fight each other?

                                                                                                                     
It is perfectly acceptable to have mutiple charging sources on a common battery bank.
Unless the load demand is sufficient, the more aggressive charging source may cause the lesser to "back off".
The C-series must have the array configured for the same voltage as the battery, while the MPPT60 array must be configured to a higher voltage.
 
Was this helpful?
What can we do to improve the information ?